- FactoryTalk Batch
- Recipe Editor
- FactoryTalk Batch Equipment Editor
- Parameters and reports with FactoryTalk Batch
- Phase class overview
- Configure phases
- Operation sequence class configuration
- Operation sequence configuration
- FactoryTalk Batch View
- PhaseManager
- FactoryTalk Batch phases in Logix Designer
- Data from FactoryTalk Batch Server
- FactoryTalk Event Archiver
- FactoryTalk Batch administration
- FactoryTalk Batch security
- FactoryTalk Batch electronic signatures
- The FactoryTalk Batch Service Manager
- The FactoryTalk Batch Server
- FactoryTalk Batch Server option configuration
- PC-based phases introduction
Edit an operation sequence class
Editing an operation sequence class updates all instances of that class, in all units containing that class. Use these instructions to edit operation sequence classes.
To edit an operation sequence class
:- SelectStart > Rockwell Software >Equipment Editor.
- Select a unit icon and then selectGo Down(
). The
Design Viewarea may display theUniticon, andClassesdisplays as the column header in theClass Viewarea. - In theClass Viewarea, right-click the operation sequence to open theEdit Operation Sequence Classdialog box.
- In theEdit Operation Sequence Classdialog box, use the tabs to create the operation sequence class:
- General
- Parameters
- Reports
- SelectOK.
Provide Feedback