UnacknowledgedEventsCt
The
UnacknowledgedEventsCt
item returns the number of unacknowledged prompts in the unacknowledged prompts list.This table shows the input and output formats for this item.
Input Format | Request: UnacknowledgedEventsCt | |
Output Format | The UnacknowledgedEventsCt item returns in this format: <NumberOfPrompts> | |
where: | ||
Field Name | Format | Description |
<NumberOf
Prompts> | ASCII - Integer | Number of prompts currently in the unacknowledged prompts list. |
This table shows an example of the return on this request.
Example: | A request on object.GetItem(UnacknowledgedEventsCt) could return:1 |
Provide Feedback