Cross invocation
Cross Invocation is the means by which the HMI Controls pass data to, and activate, an
automation server such as an HMI or Visual Basic program. The data passed is specific to an
equipment resource selected from the
FactoryTalk Batch
Client applications. FactoryTalk Batch
provides a procedure-centric view of the batches running in the plant. The HMI provides
an equipment-centric view of these batches. If the HMI is an automation server that supports
the Cross Invocation interface, cross invocation can send equipment-specific information
about a batch to your HMI. The HMI can then act based on the data received. For example, it
may invoke a graphic specific to the selected equipment resource or information specific to
an Equipment Module’s running logic.Provide Feedback