Cross invocation overview
Cross invocation is accomplished by way of user-defined and selectable cross invocation
menu items. If configured for a selected equipment resource, the cross invocation menu items
are visible and selectable by right-clicking on the running object in the
FactoryTalk Batch
client .If a recipe step is not bound to an equipment resource the
FactoryTalk Batch
client does not display the Cross Invocation
menu when you right-click on the
step.Within the
FactoryTalk Batch
client applications, there are a number of selectable procedural elements. Each of these
procedural elements relates to a specific equipment resource. Each equipment resource may be
configured to have cross invocation strings (defined on the Cross Invocation
tab of
any configurable equipment resource in the area model). Procedural Element > Equipment Resource > Cross Invocation Strings
Each cross invocation string defines:
- The text for displaying theCross invocationmenu item.
- The data for passing to the automation server.
This table shows the various equipment resource for which a selected procedural element is linked. For cross invocation to be implemented, the cross invocation strings must be configured for the equipment resource.
Procedural elements | Corresponding equipment resource |
|---|---|
Batch | Process Cell (Procedure) |
Unit (Unit Proc or Operation) | |
Batch | Process Cell (Procedure) |
Unit (Unit Proc or Operation) | |
Unit Procedure | Unit |
Operation | Unit |
Recipe Phase | Phase |
Batch | Process Cell (Procedure) |
Unit (Unit Proc or Operation) | |
Unacknowledged Prompts | Phase |
Process Cell | Process Cell |
Unit | Unit |
Phase | Phase |
Recipe | Process Cell (Procedure) |
Unit (Unit Proc or Operation) | |
Process Cell | Process Cell |
Unit | Unit |
Phase | Phase |
Resource | Resource |
N/A | N/A |
Phase | Phase |
Provide Feedback