FactoryTalk Batch Server Details dialog box - PCD Communications tab
The
PCD
Communications
tab is used to monitor the FactoryTalk Batch
Server communication status and any data servers that are communicating with the server. Verification of all tags, phases, and equipment operation sequences associated with the current area model is also performed.The
PCD Communications
tab displays these components:Field | Definition |
|---|---|
Data Server Status | Lists of all configured data servers in the area model and the communication status between FactoryTalk Batch and these data server(s). |
Tag Verify Status | Indicates if the verification function is READY, IN PROGRESS, or COMPLETED. |
Tag Verify Verified | Indicates the number of tags, phases, and equipment operation sequences that the server processed during tag verification. |
Tag Verify Bad | Indicates the number of tags, phases, and equipment operation sequences that the server was unable to verify. Bad tags, phases, and equipment operation sequences indicate either the data server cannot supply the data requested by the FactoryTalk Batch Server or the data was not of the expected type. |
Tag Verify Total | Indicates the total number of tags, phases, and equipment operation sequences. |
Start | Starts the verification process. |
Stop | Stops the verification process. |
Provide Feedback