FactoryTalk Batch Server Details dialog box
The
FactoryTalk Batch
ServerDetails
dialog box displays an overview of the current system’s status and the
current running area model. The area model file referenced is specified in the Server
Options
dialog box accessed from FactoryTalk Batch Equipment Editor
. The FactoryTalk Batch
ServerDetails
dialog box is organized into five tabs.Provide Feedback