FactoryTalk Batch Server Details dialog box - Messages tab
The
Messages
tab is used to monitor FactoryTalk Batch
Server log information. The messages displayed in the three sections are the most recent messages written to the server log by the server.The
Messages
tab shows:Field | Definition |
|---|---|
Info | The most recent Info -type entry in the log file. Info entries are log entries recorded as a part of the normal execution. |
Warning | The most recent Warning -type entry in the log file. Warning entries indicate that a minor irregularity the system detected. The irregularity was handled by the system or the system is not sure of the occurrence’s implications. |
Severe | The most recent Severe -type entry in the log file. Severe entries indicate that the system encountered a severe error condition. The system handled the situation as best it could. |
Provide Feedback