FactoryTalk Batch Server Details dialog box - View Communications tab
The
View
Communications
tab is used to monitor the number of Dynamic Data Exchange (DDE), Component Object Model (COM) and Open Platform Communications (OPC) conversations taking place between the FactoryTalk Batch
Server and Client software.The
View Communications
tab shows:Item | Definition |
|---|---|
DDE Connections | The number of DDE connections attached to the FactoryTalk Batch Server. |
COM Connections | The number of COM connections attached to the server. |
OPC Connections | The number of OPC connections attached to the server. |
Items | The number of connection items the server currently supports. |
Provide Feedback