FactoryTalk Batch Server Details dialog box - General tab
The
General
tab lists data on the number of batches and prompts being currently handled by the FactoryTalk Batch
Server, as well as the Windows time on the server, the time the batch server started, and the name and creation date of the current area model.The
General
tab shows:Field | Definition |
|---|---|
Batch Count | The number of batches loaded in the FactoryTalk Batch Server. |
Prompts Count | The number of prompts currently existing within all batches. |
Version | The version number of the FactoryTalk Batch Server. |
Time | The time as specified by Windows on the FactoryTalk Batch Server. |
Started at | The time the FactoryTalk Batch Server started. |
Area Model File Name | The name of the currently active area model. |
Area Model Date | The file date of the currently active area model at the time of FactoryTalk Batch Server startup or the last update. |
Provide Feedback