The FactoryTalk Batch Service Manager

The
FactoryTalk Batch
Service Manager is used with the
FactoryTalk Batch
Server,
FactoryTalk Batch View
Server, and
FactoryTalk Event Archiver
, when
FactoryTalk Event Archiver
is configured as a Windows service. The Service Manager manually starts and stops the
FactoryTalk Batch
Server and manually starts, pauses, continues or stops
FactoryTalk Event Archiver
services. The Service Manager accesses the
Batch Server Statistics
dialog box, which gives access to COM server information, COM client status, error information, and other
FactoryTalk Batch
Server information.
TIP:
To command the
FactoryTalk Batch
Server,
FactoryTalk Batch View
Server, or
FactoryTalk Event Archiver
services, you must have local administrator privileges on the computer where the server and/or
FactoryTalk Event Archiver
services are installed. If you do not have local administrator privileges, you will have view-only privileges.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal