Add a custom service
Define a custom service to command the
FactoryTalk Batch
Server and FactoryTalk Event Archiver
services using the FactoryTalk Batch
Service Manager. To make a service available to the Service Manager, you must enter the
file name of the executable for the service in a service registry key. This key is located
at:HKEY_LOCAL_MACHINE\SOFTWARE\BATCHCTL\Services
To add a custom service
:- In the Registry Editor, select theHKEY_LOCAL_MACHINE\SOFTWARE\BATCHCTL\Servicessubkey.

- From theEditmenu, selectNew > Key. A new key folder is added.
- Enter theKey Namewithout the file extension.
Provide Feedback