What is PhaseManager?

In
FactoryTalk Batch Equipment Editor
, create a phase class to represent a group of equipment that performs a minor processing activity in a manufacturing plant, and create a phase when a specific instance of a phase is added to a unit.
PhaseManager
is a collection of features in
FactoryTalk Batch
,
Logix Designer
, and an addition of capabilities in the
Logix 5000
family of controllers that extend the concept and definition of phases to the
Logix Designer
software and the
Logix 5000
family of controllers.
An equipment phase is a special program. A state machine built into the program manages the state of the equipment phase. The state specifies which routine the phase executes. The phase can be commanded to change states, and change the routine it is executing. Equipment phase programs have input and output parameters. Parameters can be configured as
Sequencing
parameters, marking these tags as requiring data to be supplied from an internal sequencer (
Equipment Sequence
Manager) or external sequencer (FTBatch).
PhaseManager
adds an equipment phase object to the
Logix 5000
family of controllers and gives the ability to create equipment phases in the
Logix Designer
programming software. Create or update equipment phases in
Logix Designer
by adding or modifying them directly in the project, or by synchronizing the project with an area model that contains
PhaseManager
phases. Likewise, create or update phases in the area model by synchronizing with a
Logix Designer
project file that contains
PhaseManager
equipment phases.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal