PhaseManager

PhaseManager
is a collection of features that integrates the
FactoryTalk®
Batch software with the Studio 5000
Logix Designer
™ application and the
Logix 5000™
family of controllers. The integration of these products simplifies the configuration and maintenance of the
FactoryTalk Batch
automation system, provides a superior means of communication between the
FactoryTalk Batch
Server and the
Logix 5000
controller, and significantly reduces the programming effort required to develop the phase logic code that resides in the
Logix 5000
controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal