How PhaseManager works in a FactoryTalk Batch system

PhaseManager
features work together to provide a seamless workflow that improves the designing, troubleshooting, and commissioning phases of the development life cycle. This discussion includes some background information about the components of
FactoryTalk Batch
systems and how
FactoryTalk Batch
terminology and concepts are implemented in
FactoryTalk Batch
and
Logix Designer
.
In a
FactoryTalk Batch
system using
PhaseManager
, the
FactoryTalk Batch
Server provides batch control, including recipe execution, allocation and arbitration of equipment, binding of resources, and generation of journals. Use
FactoryTalk Batch Equipment Editor
and
FactoryTalk Batch Recipe Editor
to configure the
FactoryTalk Batch
system. Use
Logix Designer
to program the phase logic code that defines the behavior of equipment phase states, including Running, Stopping, Aborting, Holding, Restarting, and Resetting.
PhaseManager
links a phase in
FactoryTalk Batch Equipment Editor
to a corresponding equipment phase and its phase logic in
Logix Designer
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal