Common Industrial Protocol (CIP)
PhaseManager
uses the Common Industrial Protocol (CIP) as the communication mechanism between the FactoryTalk Batch
Server and the Logix 5000
controller. In FactoryTalk Batch
, each Logix 5000
controller is represented as a CIP data server that was added and configured in FactoryTalk Batch Equipment Editor
. Logix5000
CIP data servers require FactoryTalk® Linx
for the CIP communications from the FactoryTalk Batch
Server to the controller.
The
FactoryTalk Batch
Server and Logix Designer
communicate with the Logix 5000
controller by sending and receiving CIP (Common Industrial Protocol) messages through FactoryTalk Linx
.Provide Feedback