Area model PhaseManager configuration

Use
FactoryTalk Batch
with
PhaseManager
to configure the area model in
FactoryTalk Batch Equipment Editor
, or develop the phase logic in
Logix Designer
. If designing an entire
FactoryTalk Batch
system, use
FactoryTalk Batch Equipment Editor
to create an area model that describes the capabilities of the equipment, down to the phase level, and optionally use the synchronization feature to create corresponding equipment phases in the
Logix Designer
project file.
This section describes how to configure data servers and phases in
FactoryTalk Batch Equipment Editor
so these
PhaseManager
features can be used:
  • CIP for
    FactoryTalk Batch
    Server communications to the
    Logix5000
    controller
  • Synchronization of phases in the
    FactoryTalk Batch
    area model with the
    Logix Designer
    project file
  • Ability to open phase logic in
    Logix Designer
    from the phase in
    FactoryTalk Batch Equipment Editor
    TIP:
    To fully use the
    PhaseManager
    features, install
    FactoryTalk Batch Equipment Editor
    and
    Logix Designer
    on the same computer.
To configure the
FactoryTalk Batch
system with
PhaseManager
:
  • Add
    Logix5000
    CIP data servers
  • Assign a
    Logix5000
    CIP data server to
    PhaseManager
    phases
After these configuration tasks are completed, if the
Equipment Phase
s in
Logix Designer
have not already been created, synchronize the
FactoryTalk Batch
area model with the
Logix Designer
project file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal