Intended audience
The information in this guide is for
FactoryTalk Batch
system designers, process engineers, and control engineers who are using PhaseManager
to develop a batch automation system with FactoryTalk Batch
and Logix Designer
to develop phase logic for Logix 5000
controllers.PhaseManager
can also be used by Logix Designer
users who do not use FactoryTalk Batch
and only want to create sequence routines and develop code for a specific piece of equipment that may be incorporated into a FactoryTalk Batch
system. In this case, see the Logix Designer
online help for information on how to use Logix Designer
with PhaseManager outside the context of a Batch system.Provide Feedback