FactoryTalk Batch features
PhaseManager
adds these features to the FactoryTalk Batch
software:- Common Industrial Protocol (CIP) supportTheFactoryTalk BatchServer can sequence equipment phases inLogix 5000controllers using the industry standard CIP (Common Industrial Protocol). InFactoryTalk Batch Equipment Editor, add aLogix5000CIP data server for eachLogix 5000controller that containsPhaseManagerequipment phases.
- Equipment phase synchronizationSynchronize the area model inFactoryTalk Batch Equipment Editorwith the project file inLogix Designer. Create or update an equipment phase once in either application and add or update it to the other application by synchronizing theFactoryTalk Batcharea model with its correspondingLogix Designerproject file.
- Navigation fromFactoryTalk Batch Equipment Editorto phase logic in aLogix DesignerprojectDirectly navigate from a phase inFactoryTalk Batch Equipment Editorto corresponding phase logic in theLogix Designerproject file.
Provide Feedback