PXRQ instruction values
This table displays a list of all the requests the phase logic can issue to the
FactoryTalk Batch
Server with the PXRQ instruction:External Request | Data Value Array Element | Value | Description |
|---|---|---|---|
Download Input Parameters | DINT[0] | 0 | Download all input parameters |
Download Input Parameters | DINT[0] | Parameter ID | Download a single input parameter |
Download Input Parameters | DINT[0] | Parameter ID of the first parameter | Download a range of input parameters |
DINT[1] | Number of parameters to download | ||
Download Input Parameters Subset | DINT[0] | 1 | Download input parameters configured for download on start |
Download Input Parameters Subset | DINT[0] | 2 | Download input parameters configured for download on transfer of control |
Download Output Parameter Limits | DINT[0] | 0 | Download all report limits |
Download Output Parameter Limits | DINT[0] | Report ID | Download the report limits configuration for a single report |
Upload Output Parameters | DINT[0] | 0 | Upload all reports |
Upload Output Parameters | DINT[0] | Report ID | Upload a single report |
Upload Output Parameters | DINT[0] | Report ID of the first report | Upload a range of reports |
DINT[1] | Number of reports to download | ||
Upload Output Parameters Subset | DINT[0] | 1 | Upload reports configured for upload on terminal state |
Upload Output Parameters Subset | DINT[0] | 2 | Upload reports configured for upload on transfer of control |
Send Message to Operator | DINT[0] | Message ID | Send a message to the operator. In the FactoryTalk Batch View , the message displays in the Phase Summary window. |
Clear Message to Operator | not applicable | not applicable | Clears the currently displayed message |
Acquire Resources | DINT[0] | Equipment ID | Acquire a single resource |
Acquire Resources | DINT[0] | Equipment ID | Acquire multiple resources |
DINT[1] | Equipment ID | ||
DINT[2] | Equipment ID | ||
Release Resources | DINT[0] | Equipment ID | Release a single resource |
Release Resources | DINT[0] | Equipment ID | Release Resources |
DINT[1] | Equipment ID | ||
DINT[2] | Equipment ID | ||
Release Resources | DINT[0] | 0 | Release all currently acquired resources |
Send Message to Linked Phase | DINT[0] | message ID | Send a message to one other phase or multiple phases |
DINT[1] | number of phases to receive message | ||
DINT[2] | message value | ||
Send Message to Linked Phase and Wait | DINT[0] | message ID | Send a message to one or more linked phases and wait for a response |
DINT[1] | number of phases to receive message | ||
DINT[2] | message value | ||
Receive Message from Linked Phase | DINT[0] | message ID | Send a request to wait for a message from another phase |
DINT[1] | message value | ||
DINT[2] | message value | ||
Cancel Message to Linked Phase | DINT[0] | message ID | The FactoryTalk Batch Server cancels the message associated with the message ID. The message was previously issued using a Send Message to Linked Phase request. |
Cancel Message to Linked Phase | DINT[0] | 0 | The FactoryTalk Batch Server cancels all messages that were previously issued with a Send Message to Linked Phase request. |
Download Batch Data | DINT[0] | 1 | Download customer-assigned or automatically-generated batch ID to specified tag number. FactoryTalk Batch Server downloads an Integer value. |
DINT[1] | parameter ID in which to store the value | ||
Download Batch Data | DINT[0] | 2 | Download unique batch ID to specified tag number. FactoryTalk Batch Server downloads an Integer value. |
DINT[1] | parameter ID in which to store the value | ||
Download Batch Data | DINT[0] | 3 | Download phase ID to specified tag number. FactoryTalk Batch Server downloads an Integer value. |
DINT[1] | parameter ID in which to store the value | ||
Download Batch Data | DINT[0] | 4 | Download a value to the specified tag number indicating whether the phase is under recipe control or manual phase control. FactoryTalk Batch Server downloads:0 = Recipe Control 1 = Manual Phase Control |
DINT[1] | parameter ID in which to store the value | ||
Download Batch Data | DINT[0] | 5 | Download a value to the specified tag number indicating the current mode of the requesting phase. FactoryTalk Batch Server downloads:0 = P-Auto 1 = O-Auto |
DINT[1] | parameter ID in which to store the value | ||
Download Batch Data | DINT[0] | 6 | Download all phase parameter MIN values to the controller tags associated with those parameters. This request actually downloads values for parameters that do not have Max and Min values as defined in the Equipment Editor, parameters of type String and type Enumeration for example. For String parameters, the request downloads empty strings. For Enumeration parameters, the request downloads a value of zero (0). |
Download Batch Data | DINT[0] | 7 | Download all phase parameter MAX values to the controller tags associated with those parameters. This request actually downloads values for parameters that do not have Max and Min values as defined in the Equipment Editor, parameters of type String and type Enumeration for example. For String parameters, the request downloads empty strings. For Enumeration parameters, the request downloads a value of zero (0). |
Generate E Signature | DINT[0] | signature template ID | Generate an electronic signature request. |
DINT[1] | Defines if signature is able to be canceled: 0 = No non-zero = Yes |
Provide Feedback