Release

The
RELEASE
execute releases a resource from the operator.
The format and return for this execute includes:
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[RELEASE(
Item,UserID,OwnerID,ResourceID
)]
where:
Item
Item name as specified by the client.
UserID
User identification associated with this event.
OwnerID
ID of the operator configured in the
batchsvr.ini
file.
ResourceID
Equipment ID of the resource to be released. This value is configured in
FactoryTalk Batch Equipment Editor
.
Action
A successful RELEASE execute removes the resource from either the requester’s or owner’s list. (The owner is notified of the action and may elect to re-acquire the resource.)
Return Format
The item populates with this data:
SUCCESS: | FAIL:
<message>
| FAILED
where:
Field
Format
Description
<message>
ASCII - String
Error message appropriately formatted for operator display.
The following table shows an example of the return on this execute.
Example:
An execute string:
[RELEASE(Item,Station5/Operator,0,68)]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal