Execute reference
An
Execute
commands the FactoryTalk Batch
Server to perform some action.
TIP:
Use the List Separator and number format for language. Examples used are for English:
List Separator: ,
Number Format: 1,234.56
For Spanish, use a semicolon ( ; ) instead of a comma for the List Separator.
The formatting methods used for each Execute:
Title | Description | ||
Execute Format | Describes the input format of the Execute statement. IMPORTANT: Do NOT use spaces, unless specifically directed to do so. Use this format: svrobject . Execute strExecute .
For Example: svrobject . ACK(Item,STATION5/Operator,1,5) | ||
Action | Describes what action is a result of the Execute. | ||
Return Format | Describes that data and its format returned by the Execute. All data returns in CFTEXT format, representing either strings or integers. | ||
A list of the key characters and what they symbolize follows: | |||
<TEXT> | is | Denotes a variable. | |
< TEXT> | is | Denotes a variable which will be expanded. | |
TEXT | is | Any text that is not enclosed in the < > characters is a keyword and appears as the literal string. | |
<NullString> | is | Denotes an empty string, CString.Empty( ), unless otherwise specified. | |
\t | is | Denotes a Tab character (ASCII - 9), used as a field delimiter. A space before and after the \t is included for readability. Do NOT include the spaces when formatting the command line. | |
| | is | Used to denote an OR situation. Either the text on left of the bar, or the text to the right of the bar used as the output. | |
\crlf | is | Denotes a carriage return/line feed character which are used as a record delimiter. | |
<sp> | is | Denotes a space character (ASCII – 32). | |
Item | is | The name of the item, as specified by the client. The FactoryTalk Batch Server creates the item. The value stored in the item on the server. The client must Advise on this item and wait for an update. Follow the naming rules listed here:
| |
UserID | is | User identification that will be entered into the event journal associated with this event. For example: Machine Name/UserID . | |
Example: | Defines an example for the EXECUTE statement in this format:
Return Format Execute String | ||
TIP:
Even though
Item
is used in examples, follow the naming rules.Provide Feedback