MatSvrControl
The to reestablish communication.
MATSVRCONTROL
execute is used by the Material Server Control
dialog
TIP:
This execute is valid when
Option when Material Server Communication is lost
is set to Switch to Manual
.The format and return for this execute includes:
Execute Format | The FactoryTalk Batch Server supports an execute with this format:[MATSVRCONTROL( Item,UserID,STATE )] | |
where: | Item | Name of the item as specified by the client. |
UserID | User identification associated with this event. | |
State | 2 represents the GOOD state. Returning to the GOOD state is the only control currently available. | |
Action | A successful MATSVRCONTROL execute reestablishes communication with the Material Server. | |
Return Format | The MATSVRCONTROL execute SUCCESS:|FAIL: <message> | |
The following table shows an example of the return on this execute.
Example: | An execute string: MATSVRCONTROL(PC2matsvrcontrol,PC2/Operator,2) |
Provide Feedback