SetParm
The
SETPARM
execute sets the parameter value(s) of a control recipe step. The SETPARM
execute does not change the MATERIAL formula parameter or the MATERIAL_CLASS formula parameter on all material phases. The MATERIAL formula parameter determines how a phase is bound and material availability for binding; because of this the value must not change during recipe execution. If storing the parameter results in deviation limits being violated that require signature confirmations, then an action ID returns identifying the signatures generated as a result of the SETPARM
execute.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[SETPARM( Item,UserID,ProcedureID,ParamName,Value )] | ||
where: | Item | Item name as specified by the client. | |
UserID | User identification entered into the event journal associated with this event. | ||
ProcedureID | Unique hierarchical path name to the procedure, unit procedure, operation or phase:
| ||
ParamName | Parameter name requiring a value assignment. | ||
Value | Value to be loaded in the step’s parameter. | ||
where: | <FullPath> | is | <CreateID> | <CreateID> /t <Path> |
<Path> | is | <StepIdentifier> | <StepIdentifier> /t <Path> | |
where: | |||
Field | Format | Description | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server | |
<StepIdentifier> | ASCII – String | Step identifier (for example, Mix:1) | |
Action | A successful SETPARM execute either changes the parameter value in the specified step or queue the value change and return an action ID. As a result of deviations triggered by the potential SETPARM, the signature requests generated can be detected. | ||
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | FAILED | ||
where: | |||
Field | Format | Description | |
<ActionID> | ASCII – Integer | Action identifier associated with signature(s) generated as a result of the potential parameter value change. The parameter value does not actually change unless all signatures are successfully signed. | |
<message> | ASCII - String | Error message appropriately formatted for operator display. | |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: SETPARM(Item, Station2/View, 37/tMakeStuff1:1/tFill1:1/tDose1:1, Amount, 3.14159) Could return: SUCCESS:997 |
Provide Feedback