User_Verify
The
USER_VERIFY
execute determines if the password provided for the specified Windows user name is correct and if that user belongs to a specified Windows group. This execute verifies Windows users and groups only.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute string with USER_VERIFY as the keyword. The format of the execute string is as follows:[USER_VERIFY ( Item,UserID,Password,Group) ] | |
where: | Item | Item name on which to place the execute. |
UserID | ID of the Windows user being verified. | |
Password | Password to be checked for specified Windows user. | |
Group | Windows group name to check for user membership. Formatted as [authority \] principal , where authority is an optional computer or domain name, and principal is a Windows group name. The delimiting backslash should be omitted if the optional authority is not included. | |
Action | A successful USER_VERIFY execute determines if the Windows user and password combination are valid and if the verified user belongs to the specified Windows group. | |
Return Format | SUCCESS | FAIL | |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: USER_VERIFY (Item,Buck,Alligators,MasterRecipeViewer) Could place this data in Item for the client: SUCCESS |
Provide Feedback