GetContainerData
The
GETCONTAINERDATA
execute retrieves a list of container and lot data entries that specify container binding options for the phase to be run using manual phase control.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[GETCONTAINERDATA( Item,UserID,UnitID,EqModID, FeedType, MaterialName )] | |||
where: | Item | Item name as specified by the client. | ||
UserID | User identification associated with this event. | |||
UnitID | Unit Resource ID containing the phase to be run. | |||
EqModID | Resource ID for the phase to be run. | |||
FeedType | Type of feed the phase will be performing. This is the literal value "ADDITION" or "DISTRIBUTION". | |||
MaterialName | Name of the material that the step adds or distributes. | |||
Action | A successful GETCONTAINERDATA execute returns a list of container and lot entries that may be legally bound to. | |||
Return Format | The item populates with this data: SUCCESS: <ContainerData> | FAIL: <message> | |||
where: | ||||
<ContainerData> | is | <NullList> | <ContainerList> | ||
<ContainerList> | is | <BindEntry> | <BindEntry><ContainerList> | ||
<BindEntry> | is | <ContainerName> \t <ContainerControllerID> \t <Capacity> \t <CEU> \t <LotName> \t <Label> \t | ||
where: | ||||
Field Name | Format | Description | ||
<ContainerName> | ASCII | Container name. | ||
<Container
ControllerID> | ASCII | ID for the container. | ||
<Capacity> | ASCII | For an addition, this is the quantity of material in the container. For a distribution, this is the remaining (available) volume of the container. | ||
<CEU> | ASCII | Engineering units used to measure a container’s volume. | ||
<LotName> | ASCII | Name of the lot. | ||
<LabelName> | ASCII | Label assigned the quantity of material. | ||
The following table shows an example of the return on this execute.
Example: | An execute string: GETCONTAINERDATA(DATA,STATION5/
Operator,55,70,ADDITION,EGG_YOLK) Requesting data from DATA returns: SUCCESS:TEMP_EGG \t 27 \t 660916 \t KG \t EGG_LOT3 \t EGGS3 \crlf |
Provide Feedback