AddEvent_Instruction
The control step in an electronic batch record using the name of the equipment phase that is currently executing, the control step index, and the control step reactivation number.
ADDEVENT_INSTRUCTION
execute allows an external application to append an event associated with an e
ProcedureThe format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[ADDEVENT_INSTRUCTION( Item,UserID,Phase,Type,Desc,StepIndex,ReactivationNumber,InstructionHTML )] | |
where: | Item | Response item name as specified by the client. |
UserID | User ID entered into the event journal with this event. | |
Phase | Phase associated with this event. | |
Type | Type of event being added. | |
Desc | Description of the event being added. | |
StepIndex | Step index of the control step associated with this event. This field’s value writes to the PVALUE field in the event journal. | |
Reactivation
Number | Control step reactivation number associated with this event. | |
InstructionHTML | (optional) HTML for the instruction step. | |
Action | A successful ADDEVENT_INSTRUCTION execute places the event into the specified electronic batch record(s). The FactoryTalk Batch Server automatically completes these fields: TIME, AREA, RECIPE, PHASE_DESC, and UNIQUE_ID. If, however, the event targets a single batch, and the batch product is configured for signature confirmation of "comments", then adding the event record to the event journal is queued pending a successful signature request signoff. | |
Return Format | The item populates with this data: SUCCESS| FAIL: <message> | FAILED | |
The following table shows an example of the return on this execute.
Example: | An execute string: [ADDEVENT_INSTRUCTION(Item,Earl\ADD_SUGAR,Instruction Complete,Step Completed,1,0,<FORM>Open the big green valve</FORM>] |
Provide Feedback