CompareAreaModels
The
COMPAREAREAMODELS
execute compares the current area model to an updated area model.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this
format:[COMPAREAREAMODELS (
Item,UserID,AreaModelName
)] | |
where: | Item | The item name, as specified by the client. |
UserID | User identification associated with this event. | |
AreaModelName | Name of the updated area model .cfg file. | |
Action | A successful COMPAREAREAMODELS request compares the two area models and logs any
differences. The request also indicates if the specified area model name is
considered legal for an online area model change. | |
Return Format | The item populates with this data: SUCCESS:
<CompareResult>_\t<LogFile>
| FAIL:
<message>
| |
where: | ||
Field | Format | Description |
<CompareResult> | ASCII – Integer | 1=Same 2=Different: Valid for Online Area Model Change 3=Different: Not Valid for Online Area Model Change |
<LogFile> | ASCII - String | The log file details the differences between the two area models compared. |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: COMPAREAREAMODELS (Item, STATION7, ice_cream1_updated.cfg) Could return: SUCCESS:2 \t \\BTCHSYSCMPTR001\batchctl\SampleDemo1\logs\COMPARE.ICE_CREAM1_UPDATED.2017-08-07_T1655050887.LOG |
Provide Feedback