SetAllLabel
The
SETALLLABEL
execute sets the same label on all material steps within a recipe. The label helps identify specific material sublots for use. In material addition phases the label identifies specific material sublots for use. In material distribution phases, the label is applied to the material sublot distributed.The
SETALLLABEL
execute applies only to material-enabled phases.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[SETALLLABEL( Item,UserID,ProcedureID,LabelString )] | ||
where: | Item | Item name as specified by the client. | |
UserID | User identification entered into the event journal associated with this event. | ||
ProcedureID | Unique hierarchical path name to the procedure, unit procedure, operation or phase:
| ||
LabelString | Label to be stored on the phase. | ||
where: | |||
<FullPath> | is | <CreateID> | <CreateID> /t <Path> | |
<Path> | is | <StepIdentifier> | <StepIdentifier> /t <Path> | |
where: | |||
Field | Format | Description | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server. | |
<StepIdentifier> | ASCII – String | Step identifier (for example, Mix:1) | |
Action | A successful SETALLLABEL execute either changes the label values in the specified step(s), or queue the change(s) and return an action ID from which the signature requests generated can be detected. | ||
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | ||
where: | |||
Field | Format | Description | |
<ActionID> | ASCII – Integer | Action identifier associated with signature(s) generated as a result of the potential parameter value change. The parameter value will not actually change unless all signatures are successfully signed. | |
<message> | ASCII - String | Error message appropriately formatted for operator display. | |
The following table shows an example of the return on this execute.
Example: | An execute string: [SETALLLABEL(Item,Station5\Operator,887 \t PREMIX_B, CUSTOMJOB2)] |
Provide Feedback