Remove
The
REMOVE
execute removes a batch from the batch list.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[REMOVE( Item,UserID,CreateID )] | |
where: | Item | Response item name as specified by the client. |
UserID | User identification entered into the event journal associated with this event. | |
CreateID | Unique identification number for a batch. | |
Action | A successful REMOVE execute results in the removal of the specified batch from the batch list, or in the queuing of the removal pending a signature. In order to be successfully removed, a batch cannot be in Manual mode and must be in one of these states:
| |
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | |
where: | ||
Field | Format | Description |
<ActionID> | ASCII – Integer | Action identifier associated with the signature(s) generated in response to the execute. |
<message> | ASCII - String | Error message appropriately formatted for operator display. |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: [REMOVE(Item,Station5/Operator,235)] Could return: SUCCESS:997 |
Provide Feedback