Bind
The
BIND
execute binds and unbinds a unit procedure or operation to or from a specified unit.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:
[BIND( <Item>, <UserID>, <ProcedureID>, <UnitID> )] | ||
where: | <Item> | Item name on which to place the response. | |
<UserID> | User ID who issued the execute is entered into the event journal associated with this event. | ||
<ProcedureID> | Recipe procedure path being bound to the specified unit: <FullPath> | ||
<UnitID> | Unit Resource ID binds to the step. If the recipe is a procedure, use:
Prompt (-1) and First_Available (-2) are not valid options for a unit procedure recipe. | ||
where: | |||
<FullPath> | is | <CreateID> | <CreateID> /t <Path> | |
<Path> | is | <StepIdentifier> | <StepIdentifier> /t <Path> | |
where: | |||
Field | Format | Description | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server. | |
<StepIdentifier> | ASCII – String | Step identifier (for example, Mix:1) | |
Action | A successful BIND execute results in the specified unit binding to the specified procedure or in the queuing of the bind request pending a signature. | ||
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | FAILED | ||
where: | |||
Field | Format | Description | |
<ActionID> | ASCII – Integer | Action ID associated with signature(s) generates as a result of the bind request. The bind request will not process unless all signature requests are successfully signed off. | |
<message> | ASCII - String | Error message appropriately formatted for operator display. | |
The following table shows an example of the return on this execute.
Example: | An execute string for a procedure recipe example: Bind(Item,Station2/View,34 /t sweetcream_up:1,55) An execute string for a unit procedure recipe example: [BIND(Item,UserID,35,55)] Either could return: SUCCESS:997 |
Provide Feedback