FactoryTalk Batch Server API

This information was developed to provide quick and easy access to information regarding the interface between the
FactoryTalk Batch
Server and
FactoryTalk Batch View
— the Application Programming Interface (API). It is a reference for those who want to develop custom interfaces.
The API is the interface between the
FactoryTalk Batch
Server and
FactoryTalk Batch View
or a custom user interface application. The server API allows collection of batch control system information and commands the server to take some action.
TIP:
The interface between the
FactoryTalk Batch
Server and Phase is documented in the
FactoryTalk Batch
PCD Programmer Technical Reference Guide
.
The two basic components of the server API are:
  • Items
    - An item is a named data structure accessed using the
    GetItem
    method.
  • Executes
    - An execute is a command to the
    FactoryTalk Batch
    Server to perform some action.
This diagram depicts the relationships between the various components of a
FactoryTalk Batch
system. The Component Object Model (COM) or Distributed Component Object Model (DCOM) protocol is used between
FactoryTalk Batch View
and the server. Use the COM or DCOM protocol between the
FactoryTalk Batch
Server and a custom user interface.
FTB_API_relationshipDiagram
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal