COM protocol
The Component Object Model (COM) interface allows programmers and system integrators to build applications to command the
FactoryTalk Batch
Server and read information from the server. The COM interface builds on the set of data items and execute commands in the server API. The COM interface allows FactoryTalk Batch
and C/C++ programmers to use COM or Distributed Component Object Model (DCOM) as the inter-process communications protocol. Additionally, this interface allows a synchronous programming model.The typical
FactoryTalk Batch
Server and BatchRemote
objects user is a Visual Basic
programmer either writing a custom Visual Basic
program or using a scripting language embedded within a third-party application.Provide Feedback