Objects, properties, methods, and events

An object is a combination of code treated as a unit, such as a control, form, or application. Each object is defined by a class, and the
FactoryTalk Batch
library provides two object classes,
BatchControl.BatchServer
and
BatchRemote.RemoteSupport
.
  • A property is a named attribute of an object. Properties define object characteristics such as size, color, and screen location, or they can define the state of an object, such as enabled or disabled.
  • A method is a procedure that acts upon an object.
  • An event is an action recognized by an object, such as clicking the mouse or pressing a key, for which written code responds. Events can occur as the result of a user action or program code, or can be triggered by the control. There are no events in this particular interface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal