BatchRemote object

The
BatchRemote
object and the
BatchServer
object both provide a mechanism used to interact with the
FactoryTalk Batch
Server. However, the
BatchRemote
object provides additional features, allowing easier access to the server from a remote computer. These additional features include the ability to automatically locate the server computer and time out a connection.
Automatically locating a server from a remote client means it is not necessary to specify the server’s computer name. This is especially useful as it allows client applications to be developed in a more generic manner. The server name is written to the Windows registry during a client installation and accessed by the
BatchRemote
object.
The timing out of a connection allows client applications to specify timeout periods for a call (
GetItem
or
Execute
) or for a connection. Distributed Component Object Model (DCOM) may take a significant amount of time to return an error code on a failed network. The
BatchRemote
object can minimize the time and effort required to implement error handling within the client. The timing out of a connection also provides a means to keep a client from hanging while in a connect or call for an extended period.
Within a
Visual Basic
script, dimension a
BatchRemote
object in order to use the object’s methods and properties. Like the
BatchServer
object, the
BatchRemote
object exposes only two methods:
GetItem
and
Execute
. These map directly to the items and executes that are documented within this manual. Any item referenced in this manual can be retrieved through the
GetItem
method on the
BatchRemote
object. Any execute referenced in this manual can be sent through the
Execute
method on the
BatchRemote
object.
In order to use the
BatchRemote
object, add the Batch Server Remote 1.0 Type Library to the
Visual Basic
project.
TIP:
The
FactoryTalk Batch
Server application includes the
BatchServer
object, the
Batchsvr.exe
file. The
BatchRemote
object is in the
Batchrem.dll
file. Both files are in the
\Bin
subdirectory where
FactoryTalk Batch
installs. A type library,
Batchsvr.tlb
, installs with the server and can be loaded as a reference in
Visual Basic
.
For more information on how to reference an object in a
Visual Basic
project, see the
Microsoft Visual Basic Programmer's Guide
.
Additionally, a header file,
Batchsvr.h
, used for C or C++ programming installs with the server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal