Cancel all messages
Configure the PXRQ instruction in
Logix Designer
to cancel all messages that were sent to another phase:External Request | Data Value Array Element | Value |
Cancel Message to Linked Phase | DINT[0] | 0 |
The
FactoryTalk Batch
Server cancels all messages that were previously issued with a Send Message to Linked Phase
request.Provide Feedback