Message removal
The request, the
Send Message to Linked Phase
call can be canceled by the phase logic that sent the message. The phase logic can remove the message by using the Cancel Message to Linked Phase
request. Upon receiving the Cancel Message to Linked Phase
FactoryTalk Batch
Server removes the message from the message queue and clears the request on the phase.Use the PXRQ instruction to specify the
Cancel Message to Linked Phase
external request for these types of requests:- Cancel a single message
- Cancel all messages
Provide Feedback