Cancel a single message

Configure the PXRQ instruction in
Logix Designer
to cancel a single message that was sent to another phase:
Cancel Message to Linked Phase
DINT[0]
message ID
The
FactoryTalk Batch
Server cancels the message associated with the message ID. The message was previously issued using a
Send Message to Linked Phase
request.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal