Unit Bind Prompt Acknowledge Signature request
If a Bind Ack Command Verification policy is configured in the area model and it is associated with a Signature Template, then a
Unit Bind Prompt Acknowledge Signature
request is generated when binding a Unit to a step after a prompt has been generated or prompting bind’s a Unit to a step.The following is an explanation of the modifications made to support
FactoryTalk Batch
electronic signatures:Unit Bind Execute | |
|---|---|
Batch Server | When the FactoryTalk Batch Server receives a legal Ack execute in response to a Unit Bind Unacknowledged Event, it may queue the bind selection delivery pending a Signature Request if such behavior is configured in the area model. |
Response | An ActionID is returned by the Execute used to locate the generated signature. |
Completion | When all Signature Signoffs generated by an Ack received in response to a Unit Bind UnacknowledgedEvent are completed, then the Unit Requirement binds to the Ack execute response Unit specified if the bind action is still legal. |
Cancellation | When any Signature generated by a Unit Bind Ack execute is cancelled, then the Unit Bind Ack Action is terminated and its associated incomplete Signature Requests are System Cancelled. |
Overlap | If a Unit Bind Ack execute response to a Unit Bind Prompt is received while there are existing incomplete Signature Requests generated by a prior Unit Bind Ack Action targeting the same prompt, or the Batch has a Remove Action pending , then the new execute fails. The failed execute’s response item is populated with an appropriate error message string. |
Automatic Cancellation | If the batch system cancels an UnacknowledgedEvent targeted by a Unit Bind Ack Action, then the queued Execute Action is terminated and all incomplete Signature Requests associated with the Action are System Cancelled. |
Warm Reboot | Signature Requests generated in response to a Unit Bind Ack Execute Action are System Cancelled in the event of a FactoryTalk Batch Server warm boot. |
Provide Feedback