The area module and command verification policies
The area model supports several types of command verification policies that can generate signature requests before, during, or when batch execution is complete.
Actions initiated in or through the .
FactoryTalk Batch View
, HMI Controls, e
Procedure FactoryTalk Batch
Server API, generate signature requests. For information on executes, see the FactoryTalk Batch
Server API Communication Language Reference GuideProvide Feedback