FactoryTalk Batch electronic signatures

FactoryTalk Batch
electronic signatures are electronically recorded representations of a signature and their associated data. Signature data includes time stamps, security permissions, meanings for signoffs, and comments. When a signature request is created, an entry is recorded in the Event Journal. If the signature request is user generated, a
Signature
dialog box is displayed. Additional journal entries are recorded when a signature request is completed, user canceled, system canceled, or when a signoff is successful or unsuccessful. These electronic signatures include all the components necessary for compliance with 21 CFR Part 11.
A
Signature
dialog box displays context information to the user based on the signature request type. For example, a
Command Signature
dialog box displays
Time Generated
,
Batch ID
,
Procedure ID
, and
Command
.
There are several steps involved in configuring and executing electronic signatures.
IMPORTANT:
The
FactoryTalk Batch
Server responds differently when electronic signatures are configured in the area model. Be aware of the behavior changes before a decision is made to implement electronic signatures.
The requested user information in a
Signature
dialog box is defined by the signature template configured in the area model. Signature templates determine the number of signoffs required to complete a signature request. Each signoff has associated security permissions, meaning, and may require a comment. Signature templates are used with:
  • Command Verification Policies
  • Parameter Deviation Verification Policies
  • General Usage Phase Logic Requests
  • e
    Procedure
    Step Verifications
Signature templates are used to generate signature requests displayed in
FactoryTalk Batch View
, HMI Controls, and
e
Procedure
.
Signature templates determine the credentials and number of signoffs required for steps defined as part of a Recipe Approval process.
See the
FactoryTalk Batch Equipment Editor
User Guide
for information on configuring signature templates.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal