Electronic signature security

FactoryTalk
Security is used to support
FactoryTalk Batch
Electronic Signature Signoffs. The
ESignature Network Directory
policy setting is created in the
FactoryTalk
Local Directory during
FactoryTalk Batch
installation with a default value of
True
. The value of the
ESignature Network Directory
policy setting determines whether the users and groups defined in the
FactoryTalk
Local Directory or the users and groups defined in the
FactoryTalk
Network Directory are used to assign Security Permissions to Electronic Signature Templates and validate Electronic Signature Request Signoffs.
Security Permissions for Signature Signoffs are specified when the Signature Template is created in
FactoryTalk Batch Equipment Editor
. The Security Permissions defined in the Signature Template are required to complete the Signoff(s) generated in the associated Signature Request. Each Signoff requires a UserID and a password. When a signature requires multiple signoffs, each signoff must be made using a unique UserID and password.
Signature templates are also used for Recipe Approval process signoffs, and must be configured before recipe approvals can be enabled, configured, and executed.
For more information on configuring signature templates, see the
FactoryTalk Batch Equipment Editor
User Guide
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal