Configure the ESignature network directory policy setting
The ESignature Network Directory policy setting must be set to True to enable signature signoff permission validations across a network.
IMPORTANT:
Changing the
FactoryTalk Directory
Server after creating Signature Templates causes Signoffs to fail unless the FactoryTalk
System folder is backed up and restored on the new FactoryTalk Directory
Server.To configure the ESignature network directory policy setting
:- Open the Local Directory inFactoryTalkAdministration Console.
- In theExplorertree, navigate toSystem > Policies > Product Policies > Batch > Equipment Editor > Configuration > Options.
- Right-clickOptions, and selectProperties. TheOptions Propertiesdialog box displays the available policy settings.
- Select theESignature Network Directorypolicy setting and selectTrueto use network security.
- SelectOK.
- Restart the server and client applications.
Provide Feedback