Parameter deviation verification policies
FactoryTalk Batch
parameter deviations provide automatic detection of deviations for recipe and report
parameters, automatic prompting for electronic signatures, and automatic recording of these
events in the FactoryTalk Batch
Event Journal. If a phase class parameter or report parameter is configured with a Verification method and
associated with a signature template, then a Signature Request is generated. If the
signature is user generated, then a Signature dialog box opens to the user when the defined
parameter limit values are exceeded. If the Signature Request is not user generated, then
the Signature prompt begins to flash and the Signature Request displays in the Signature
List. For information on enabling parameter limit tags, see the
FactoryTalk Batch Equipment Editor
User Guide.
TIP:
The
FactoryTalk Batch
Server does not allow batch creation if the Verification configuration in the recipe is
different from the area model Verification configuration.Provide Feedback