General usage phase logic requests

A
General Usage Signature
request is created when a General Usage Phase Logic request is sent to the
FactoryTalk Batch
Server during the execution of an automated phase. Each signature template configured in
FactoryTalk Batch Equipment Editor
has a unique template index. To generate a signature the Phase Logic request specifies the signature template index.
For information on configuring general usage phase logic requests, see
Download Batch Parameters
in the
FactoryTalk Batch
PCD Programmer Reference Guide.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal