Add Event Signature request
If a Comment Command Verification policy is configured in the area model and it is
associated with a Signature Template, then an
Add Event Signature
Request is
generated when a user attempts adding a comment to a batch. For information on the AddEvent
execute, see the FactoryTalk Batch
Server API Communication Language Reference Guide.The following is an explanation of the modifications made to support
FactoryTalk Batch
electronic signatures:AddEvent Execute | |
|---|---|
Batch Server | When the FactoryTalk Batch Server receives a legal AddEvent, AddEvent_Phase, or AddEvent_CI execute, it
checks the Area Model configuration to determine if a confirmation Signature is
required for the AddEvent action. If one is required, then a Signature Request is
generated using the specified Signature Template and the AddEvent action is queued
pending completion of the Signature Request.An AddEvent is not generated when all batches are selected. |
Response | An ActionID is returned by the execute used to locate the generated signature. |
Completion | When all Signature Signoffs associated with an AddEvent execute are completed, then the AddEvent action is handled if it is still legal. |
Cancellation | When any Signature generated by an AddEvent execute action is cancelled, then the AddEvent execute action is terminated and its associated incomplete Signature Requests are System Cancelled. |
Overlap | AddEvent executes targeted at the same batch are permitted to overlap. If the batch has a Remove Action pending, then AddEvent execute fails. |
Warm Reboot | Signature Requests generated in response to a AddEvent execute action are
restored in the event of a FactoryTalk Batch Server warm boot. |
Provide Feedback