Command signature requests
If a command verification policy is associated with a signature template, and a command is issued against a batch, a
Command Signature
request is generated and a dialog box is displayed. For example: If a HOLD command requires a signature, then when a HOLD command is issued
against a batch, an electronic signature request is generated and a dialog box is displayed.
For information on command signatures, see .
Acknowledge a Command Signature
in the
FactoryTalk Batch View
User GuideThe following is an explanation of the modifications made to support
FactoryTalk Batch
electronic signatures:Command Execute | |
|---|---|
Batch Server | When a legal command execute is received, the FactoryTalk Batch Server checks the area model configuration to determine if a signature request
is required. If yes, then the command action is queued and a signature request is
generated.Exception: ABORT Command is not queued. |
Response | An ActionID is returned by the execute used to locate the generated signature. |
Completion | When all signature signoffs generated by the queued command are complete, the command is issued to the target procedure. Exception: ABORT command is issued regardless of Signature state. |
Cancellation | When any signature is user canceled, then the queued command is terminated and all other signature requests associated with the same command action are system canceled. Exception: ABORT command cannot be canceled by the user. |
Overlap | If a command execute is received by a procedure that has incomplete signature requests for a prior command execute action, then the new command execute fails. A failed execute’s response item contains an appropriate error message. Exception: ABORT Command creating a command overlap terminates the original command action causing a system cancel instead of a failure. If ABORT overlaps with an ABORT command, then any incomplete signatures for the first command are system canceled and a new signature request is generated for the second command. |
Automatic Cancellation | When a procedure transitions to a state in which a queued command action is not legal, the command execute action is terminated, and its associated incomplete signature requests are system canceled. |
Cmd | Commands used with command verification policies are: START STOP AUTO-MODE
PAUSE HOLD RESTART
MAN-MODE RESUME ABORT
RESET CLEAR_FAILURES DISCONNECT
SEMIAUTO-MODE |
When a Command Verification Policy is configured for a command, and the same Command is issued in Manual Phase Control against a Phase, a
Command Signature
request is generated.The following is an explanation of the modifications made to support
FactoryTalk Batch
electronic signatures:Phase, Phase2, Phase3 Executes | |
|---|---|
Batch Server | When a legal command execute is received, the FactoryTalk Batch Server checks the area model to determine if a signature request is required.
If yes, then the command is queued and a signature request is generated.Exceptions:
|
Response | An ActionID is returned by the Execute used to locate the generated signature. |
Completion | When all Signature Signoffs generated by the queued command are complete, then the Command is issued to the target procedure. Exception: ABORT Command issued regardless of Signature state. |
Cancellation | When any Signature is user canceled, then the queued Command is terminated and all other Signature Requests associated with the same command action are System Canceled. Exception: ABORT Command cannot be canceled by the user. |
Overlap | If a Phase Execute is received by a procedure that has incomplete Signature Requests for a prior Phase Execute Action, then the new Phase Execute fails. If a Command Execute is received by a phase that has incomplete Signature Requests for a prior Phase Reset or Phase Disconnect, then the new Command Execute fails. The failed Execute’s response item contains an appropriate error message. Exception: ABORT Command creating a Command overlap terminates the original Command Action causing a System Cancel instead of a failure. If ABORT overlaps with an ABORT Command, then any incomplete Signatures for the first command are System Canceled and a new Signature Request is generated for the second command. |
Automatic Cancellation | When a procedure transitions to a state in which a queued Action would not be legal, the Execute is terminated, and its associated incomplete Signature Requests are System Canceled. |
Warm Reboot | Signature Requests generated in response to a Phase Execute Action are System
Canceled in the event of a FactoryTalk Batch Server warm boot. |
Provide Feedback