Phase Bind Prompt Acknowledge Signature request
If a Bind Ack Command Verification policy is configured in the area model and it is associated with a Signature Template, then a
Phase Bind Signature
request is generated when binding a phase to a material after a prompt is generated or prompting binds a phase to a material.The following is an explanation of the modifications made to support
FactoryTalk Batch
electronic signatures:Recipe Phase Bind Ack Execute | |
|---|---|
Batch Server | When the FactoryTalk Batch Server receives a legal Ack execute in response to a Recipe Phase Bind UnacknowledgedEvent, it may queue the bind selection delivery pending a Signature Request if such behavior is configured in the area model. |
Response | An ActionID is returned by the Execute used to locate the generated signature. |
Completion | When all Signature Signoffs generated by an Ack received in response to a Recipe Phase Bind UnacknowledgedEvent are completed, then the Recipe Phase is bound using the Ack execute response data specified if the bind action is still legal. |
Cancellation | When any Signature generated by a Recipe Phase Bind Ack Execute is cancelled, then the Recipe Phase Bind Ack Action is terminated and its associated incomplete Signature Requests are System Cancelled. |
Overlap | If an Ack execute response to a recipe Phase Bind Prompt is received while there are existing incomplete Signature Requests generated by a prior Ack to the same prompt, or the Batch has a Remove Action pending, then the new execute fails. The failed execute’s response item is populated with an appropriate error message string. |
Automatic Cancellation | If the batch system cancels an UnacknowledgedEvent targeted by a Recipe Phase Bind Ack Action, then the queued Execute Action is terminated and all incomplete Signature Requests associated with the Action are System Cancelled. |
Warm Reboot | Signature Requests generated in response to a Recipe Phase Bind Ack Execute Action are System Cancelled in the event of a FactoryTalk Batch Server warm boot. |
Provide Feedback