EquipmentModel

The
EquipmentModel
item returns the path and file name of the equipment model in use.
This table shows the input and output formats for this item.
Input Format
Request:
EquipmentModel
Output Format
The EquipmentModel item returns in this format:
<PathName>
Field Name
Format
Description
<PathName>
ASCII – String
Path and file name of equipment model in use.
This table shows an example of the return on this request.
TIP:
A request on
object.GetItem(EquipmentModel)
could return:
\\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH\SAMPLEAPP\RECIPES\ICE_CREAM.CFG
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal