Upload container data into container currently in use
This request fails (without notice) if the data is read-only
Configure the PXRQ instruction to upload container data about the container the phase is currently running against.
External Request | Data Value Array Element | Value |
|---|---|---|
Download Material Manager Data Container in Use | DINT[0] | 1 |
DINT[1] | Data to upload into (attribute ID). | |
DINT[2] | Report tag address of the value stored in the material database. |
Provide Feedback