Batch Server tab

The
Batch Server
tab allows you to select and/or configure
FactoryTalk Batch
Server options (including the hold propagation type), watchdog communications timeout settings,
FactoryTalk Event Archiver
log file size, minimum disk space required to add a batch, default batch ID, and whether to enable/disable event journal signatures.
FTB_Admin_Server_Opts_BatchServer2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal